Machines and plants, Linear slides, Pneumatic cylinders, Handling modules, Electro-mechanical drives
Higher loading speed with simultaneous protection of the loading mechanism for lathes in the automotive industry
ACE TUBUS profile dampers protect the integrated loading station on a new high speed machining center. The ACE TUBUS damper is designed to prevent overrun on the high speed loading station of a Camshaft machining centre used in the automobile industry. In the event that the drive train fails during operation or incorrect data is inputted the ACE TUBUS damper absorbs the impact preventing costly damage to the machine. The TA98-40 TUBUS damper impressed engineers with this exceptionally long service life in operation. When used as an emergency stop the TUBUS damper can absorb up to 73 % of the impact energy.
Brake components for pneumatic linear modulesPneumatic linear modules in miniature slide systems ensure high speeds with constant repeat accuracy. In this design, pneumatic end-of-travel...
Industrial Gas Springs – Push Type - GS-8 to GS-70
TUBUS damping for more sustainable sortingA sorting plant for copper from Wieland-Werke AG is used to separate the metal-dross mixture. During the separation process the metal runners with...