Increase speed and reduce downtime with automatic sealing of screw caps
Miniature Shock AbsorbersMC150 to MC600
Pump spray bottle being handled by friction wheels, detail of our miniature shock absorbers for higher cycle rates and perfect end position protection to the left Copyright: Metallatelier GmbH, Deggenhausen, Germany
Miniature Shock Absorbers MC150-MC600
Pump spray bottle being handled by friction wheels, detail of our miniature shock absorbers for higher cycle rates and perfect end position protection to the left Copyright: Metallatelier GmbH, Deggenhausen, Germany
Safety and productivity in harmony with miniature shock absorbers from ACE
A customer of Metallatelier GmbH needed a special machine for automatically capping bottles with disinfectant during the COVID-19 pandemic. The German company optimized a proven design for this purpose. This is also because the designers chose our miniature shock absorbers for end position damping and limiting the contact roller gripping movement. At the bottom, two MC150M brake the pneumatic linear slide, serve to limit the closing movement in the end position and also protect the entire construction in the event of an accident. At the top, a harder designed single type MC150MH ensures saved space and safe deceleration of the slide.
Matching Applications
Industrial Shock Absorbers - MA/ML33 to MA/ML64
Securing linear drive units mechanicallyGSI Helmholtzzentrum für Schwerionenforschung in Darmstadt, Germany, operates a unique accelerator for heavy ions. Currently, the international...
Impact damping for heavy industrial wood sawsIn this application, SLAB damping mats SL-030 with a thickness of 0.49 inch were screwed between two steel sheets over the entire surface in order...
Pneumatic rod clamping for hydraulic pressesWith the help of hydraulic presses, cut ceramic parts are manufactured during the week. So that the rods of the upper and lower stamping plate do...
Industrial Gas Springs – Push Type - GS-8 to GS-70